NumericFunctions.Regex occurrences function
Returns the number of times a pattern occurs in another string
Format
ANSI-SQL Format:
OCCURRENCES_REGEX( Pattern, [ FLAG Options ] IN Subject [ FROM Start ] )
Remarks
Returns the number of times the Pattern occurs in Subject.
Pattern is the regular expression string to search for. For more information on regular expression patterns, refer to Regular Expressions.
If specified, the Option argument changes the pattern matching behaviour. For more information on regular expression options refer to Regular Expression Option Flags.
Subject is the string to be searched.
If specified, the Start argument is the 1-based offset into Subject to start the search. If Start is less than 1 or greater than the length of Subject, the function returns -1. If Start is not specified, the starting position is assumed to be 1, which is the first character in Subject
OCCURRENCES_REGEX( 'a.b' IN 'aab abb acb adb' ) returns 4